Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

SPEEDVAL KIT HALF-BRIDGE MOTHERB : MOD-MB-HB-0900V-40A Single phase inverter testing

oming0731
oming0731 Contributor Level 1
edited May 2024 in General

Dear all,

I have question about SPEEDVAL KIT HALF-BRIDGE MOTHERB : MOD-MB-HB-0900V-40A.

I'd like test sinlge phase inverter using it.

However, there is no reference about it in the datahseet.

I think it is possible to test single phase using the speedval kit.

I have questions about it.

Question 1) DC link cap

One thing I concered is that DC link cap.

Does it include DC link cap or not? more specific, the DC link cap should be splited by VDC/2.

Question 2) Modify the speed kit

Also, I'd like to modifiy the test kit to auxiliary resaonant commutated pole inverter(ARCP).

Red one is the Speed kit and other things are the external one.

Have you tried like this circuit? I think it is possible. Do you have any concern about the configuration?

image.png

Question 3) Dspace.

I'd like to use DSpace as the gate signal function generator.

This is becauase the mother board can suport external fuction generator using BNC cable.

Have you test it using Dspace?

Best regards,

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • AAnders
    AAnders Wolfspeed Admin - Contributor Level 4

    Hello,

    Thanks for your inquiry. Here are the answers to your questions:

    1. The DC link consists of four 12uF 1100V film capacitors in parallel. There is no mid-bus.
    2. The configuration for the auxiliary resonant commutated pole inverter is not possible using the standard MOSFET daughter cards. The MOSFET cards are designs as a standard half-bridge, meaning that the source of the high-side is connected to the drain of the low-side. In the topology you mentioned, I believe you would need either a common-source or a common-drain configuration in order to control the AC current.
    3. We have not used DSpace, but you can use any source to generate the PWM signals as long as you can provide a 0-5V PWM signal to the BNC.

    Thanks,

    Adam

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.