Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

About 3D data inside CAB450M12XM3

TKishi
TKishi Contributor Level 2
edited October 2023 in Module Products

Hi 

My customer has question.

We would like your cooperation as this is a major point in the selection process.

The customer needs 3D data inside the module to simulate the heat generated by the module.

The results of thermal simulation are important because if heat generation can be suppressed, the weight of the product's heat dissipation mechanism can be reduced.

If 3D data is not available, we would like information such as the size of the bare die, the material, length, and thickness of the insulating substrate and wires.

Best regard

T Kishi

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • PaulKanatzar
    PaulKanatzar Wolfspeed Employee - Contributor Level 2
    edited September 2023

    T Kishi,

    The information is only available under NDA. I will reach out privately with more information.

    Thanks,

    -Paul

  • TKishi
    TKishi Contributor Level 2

    Hi Paul

    Thank you for reply.

    I understood that NDA is required.

    However, the heat generation of the module is an important selection point for customer. Also, the customer plans to consider replacing it in October, so there is no time.

    I don't need all the 3D data, just the material (thermal conductivity) and dimension (WLH) information of the part structure, so would it be possible to support this?


    If necessary, we can provide individual support, so please contact me directly via email.

    tatsuro_kishimoto@marubun.co.jp


    Best Regard

    T Kishi

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I will close this discussion for now as our team has reached out to you privately to help solve your query. If you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.