Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

LTspice model C2M0040120D

Amaury
Amaury Contributor Level 1
edited February 2024 in Discrete Products

Hello,

I'm currently working on simulation with Ltspice and C2M0040120D model, and to be sure that my circuit was working I try to remake some graphic of the data sheet. But wasn't able to have the good value, so I change my circuit but nothing changes, so I test with another Mosfet, the C2M0080120D and with this Mosfet I found the correct value. So I want to know if it's my circuit the problem or if this can be the model of the C2M0040120D.

Thank you for your time and support,

Amaury

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • sparasaram
    sparasaram Wolfspeed Employee - Contributor Level 1

    Hello Amaury,

    Thank you for your question. I want to understand your question better. 

    1) What graphic of the datasheet were you planning to remake?

    2) I see that you have utilized two different junction temperatures: -55C for C2M0040120D and 25C for C2M0080120D. Is this intentional?

    3) I also see that in the C2M0040120D case you utilized 20V (positive) gate voltage whereas for C2M0080120D you use only 10V. Is this intentional?

    More details would help me debug the issue better. 

    Thank you for your patience

    Sparasaram

  • Amaury
    Amaury Contributor Level 1

    hello,

    Here are my answers.

    For the first question, I want to remake all the graphics of the datasheet except those that don't need ltspice simulation. And for questions 2 and 3, I just took photos of the circuits in the state they were in to remake certain graphics, so that's why the C2M0040120D has a Tj of -55°C and a Vgs=20V and that the C2M0080120D is 25°C with Vgs=10V.

    Thank you for your time and support.

    Amaury

  • Amaury
    Amaury Contributor Level 1

    I neglected to mention that the purpose of my request is not the C2M0080120D; rather, it was to demonstrate that, while using the C2M0040120D, I got inconsistent results, while using the C2M0080120D, the results were in line with the datasheet.

    Amaury

  • sparasaram
    sparasaram Wolfspeed Employee - Contributor Level 1

    Hi Amaury,

    Thank you for your patience, I do see the issue you are talking about. I can see the IV curves simulated ones don't match well with the datasheet specified values. It is an issue with the ltspice model.

    Also the spice model for the C2M0040120D has been made a while back. I would like to revisit and possibly create a one off for your simulation purposes.

    Please provide me with a couple of days of time to provide you with a newer model.

    Thank you,

    Sparasaram

  • Amaury
    Amaury Contributor Level 1

    Hi,

    Thank you for those details, and thank you also for revisiting the LTSpice model. I can wait a couple of days for the models.

    Have a nice day.

    Amaury

  • sparasaram
    sparasaram Wolfspeed Employee - Contributor Level 1

    Hi Amaury,

    I apologize for the delay, please find the attached model generated for C2M0040120D. I believe this model is much closer to the datasheet parameters then the existing version. Please let me know if you have any questions.

    Thank you,

    Sparasaram


  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.