Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CPM3-1200-0013A

meet_panchal
meet_panchal Contributor Level 1
edited February 2024 in Bare Die Products

Hello,

I am looking for CPM3-1200-0013A detailed data sheet with rise time and fall time data or dv/dt for CPM3-1200-0013A bared die MOSFET.

any help would be appreciated.

Thank you.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • DHofmann
    DHofmann Wolfspeed Employee - Contributor Level 2

    Hello Panchal,

    the switching times depent on package layout, package inductances, DC link and load inductance.

    As an indicator you can use https://assets.wolfspeed.com/uploads/2024/01/Wolfspeed_C3M0016120K_data_sheet.pdf

  • meet_panchal
    meet_panchal Contributor Level 1
    edited February 2024

    Thank you for your response.

    What do you mean by as an indicator, attached MOSFET data sheet is different from which we are using.

    can you please explain further?

    please find attached data sheet.


  • DHofmann
    DHofmann Wolfspeed Employee - Contributor Level 2

    The datasheet I shared is from 16 mO device but you are looking for 13 mO.

    Rise time and fall time are shown in the datasheets of our discrete devices. Those values can be taken as indicator of tr and tf . The 13 mO device is a bit slower but as said before, tr and tf depend on DC link voltage, layout the die is assembled in as well as output inductance.

  • meet_panchal
    meet_panchal Contributor Level 1

    Thank you for the information.

    would you provide us with the rise time and fall time information with this information we have.


  • DHofmann
    DHofmann Wolfspeed Employee - Contributor Level 2

    Estimated parameter because tr and tf depend on module layout.

    Room temperature ; Vdc = 800 V ; Id = 100 A

    tr ~ 40 ns

    tf ~ 30 ns

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.