Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

What is the shelf life of CAB011M12FM3T thermal interface material

jiten000
jiten000 Contributor Level 1
edited February 2024 in Module Products

Hi,

I want to know the storage life of CAB011M12FM3T with Pre-Applied Phase Change Thermal Interface Material.

Is the performance of TIM affected if module is stored for a long time before attaching it to the heat sink?

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • ArunA
    ArunA Wolfspeed Employee - Contributor Level 2

    Hi Jiten,

    The recommended storage condition for Wolfpack modules with pre-applied TIM is 12 months as explained in this application note section 3.2. Longer periods of storage may lead to drying out of the TIM which can lead to the TIM not spreading out uniformly when attached to a heatsink and this can result in performance issues. Hence it is always advised to follow the storage recommendations listed in the note.

    Regards,

    ArunA

    jiten000
  • jiten000
    jiten000 Contributor Level 1

    Hi Arun,

    Thanks.

    If possible, can you also share the photo of original packaging of PATIM modules.

    Regards,

    Jitendra

  • ArunA
    ArunA Wolfspeed Employee - Contributor Level 2

    Hi Jitendra,

    Here is a picture of the packaging of the FM/GM Wolfpack modules with PATIM. A GM module is depicted here, but FM modules are also shipped in the same packaging.

    image.png

    Regards,

    ArunA

    jiten000
  • jiten000
    jiten000 Contributor Level 1

    Thanks, have a good day.

This discussion has been closed.