Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Model can not work on PLECS

WEN
WEN Contributor Level 2
edited July 2024 in Discrete Products

Hello WS,

I simulated the C3M025065J1 switching behavior by PLECS, but has no output, could you help to check the model is ok? thank you! attached is my circuit.

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • Urvi_Ahluwalia
    Urvi_Ahluwalia Wolfspeed Employee - Contributor Level 2
    edited May 2024

    Hi WEN,

    I suggest the following changes to your simulation:

    1. Pulse generator should give out 1/0 output, not +15/-3. The gate of the FET model needs 1/0 input.
    2. Please add anti-parallel diodes to the FET and add the body diode model of C3M025065J1 to it as shown here. image.png

    While these two changes should help you run the simulation, I'd like to warn that PLECS simulations waveforms are ideal. Ringing and overshoots are not considered. Therefore, if you'd like to see effect of parasitics and dv/dt values based on the gate voltages, I recommend using a Spice simulation for DPT circuit.

    I am attaching your model after making the changes I recommended above. I hope this resolves your query.

    Regards,

    Urvi

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.