Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CRD-22AD12N at 480V

Steve77
Steve77 Contributor Level 1
edited August 2024 in General

We like to develop a 22kW active front end with liquid cooling. Both CRD-22AD12N and CRD-25BDA6512N-K seem to be good choices. Since we need both single phase 230V and three phase 380-480V input none of them is a perfect match but we think the former one is the best candidate to start with.

What firmware modifications are needed to operate at 480V input?

We need +50% overload capacity for 2 seconds? With liquid cooling do you think the reference design can handle this as is or what improvements are needed?

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • FrankWei
    FrankWei Wolfspeed Employee - Contributor Level 2

    Hi Steve,

    Yes, to support 480Vac input, firmware modifications will be required. Please try to but we can not share more details about the FW update here. could you please contact Wolfspeed local FAE or sales team. then the Wolfspeed engineering team can try to support it. thank you for your understanding.

    +50% overload capacity for 2 seconds, With liquid cooling, it is possible.

    Regards,

    Frank

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.