Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Gate driver for C3M0021120K

SerafinoConvertini
SerafinoConvertini Contributor Level 1
edited September 2024 in Discrete Products

Hi,

I chose the mosfet C3M0021120K for my application but I'm having some difficulties to search for an appropriate gate driver. The mosfet has the kelvin source. The gate drive should have a maximum power of 1W. Does anyone suggest a correct part number for the gate driver?

Thanks in advance

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • Julius_R
    Julius_R Wolfspeed Employee - Contributor Level 3

    Greetings:

    If you can share a little information about your application, it will help us recommend a driver suitable for your requirements. Is this an automotive or industrial application? Does your application require short circuit protection? Are you looking for a lower cost driver that has just the basic features or one with more features such as adjustable slew rate, adjustable blanking time (desat/overcurrent), etc.

    Julius R

  • SerafinoConvertini
    SerafinoConvertini Contributor Level 1

    Hi Julius, the main difficult is about the connoection of Kelvin source. May application is industrial, I need also a short circuit protection, nothing adjustable. Thanks

  • Julius_R
    Julius_R Wolfspeed Employee - Contributor Level 3

    The Kelvin source pin is what will connect to your gate drive loop. The power source pin is what connects to the power loop. With proper layout, the kelvin source pin will allow you to achieve much lower switching losses. If you are new to designing with a kelvin source I recommend you take a look at some of the layouts on our reference designs. The layout files are all available on our website.

    I am attaching a link to another thread that contains some slides that will aid you in gate driver selection. The UCC21710 or ADuM4146 would be potential options as they both have short circuit protection. Please let me know if you have any additional questions.

    Julius R

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.