Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Simulation of stray capacitances (Cgs, Cgd,Cds) with double pulse test Continue

nugzari
nugzari Contributor Level 2
edited October 2024 in Module Products

Thank you for your explanation. However, I did not understand what you mean by ags = 0.5 and Cgs is scaled to 0.5.
Assuming Cgs= 12nF. If I apply ags = 0.5, what value will Cgs take?

Can't I just do cgs, cgd or cds sweep. For example Cgs = {10nF, 20nF, 30nF} and look at the progression of Vmid, Ids, IloadInd?

thank you, and sorry for later feedback.

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • Bdeboi
    Bdeboi Wolfspeed Employee - Contributor Level 3

    Hello,

    As mentioned in the other thread, Cgs is a voltage-dependent variable, so it is not associated to a single value. You could replace the Cgs implementation in the model with a static capacitance quite easily, but in the model's current implementation the ags variable will scale the entire Cgs function. For example, consider the CGS curves below for three different values of ags.

    image.png

    Hope this helps.

    Brian

  • nugzari
    nugzari Contributor Level 2

    Thank you very much.

    How can I replace Cgs implementation in the model with a static capacitance?

    Which of both implementation would you recommend, current implementation or implementation with static capacity and why?

    Then can you please tell me how to plot Cgs vs Vgs with DPT - Simulation?

  • Bdeboi
    Bdeboi Wolfspeed Employee - Contributor Level 3

    Hi there,

    First, open the .lib file that contains the model contents.

    Second, find the module .subckt model you are simulating (below is for a CAB450M12XM3) and identify a few parameters from the statement: AFm, die, and level. AFm is the number of MOSFETs in parallel. 'die' is the die model being used, and level is the complexity. By default, level is set to 3, but can be changed to 1 or 2 in the SPICEline.

    image.png

    In this case, if level=3, then the die model we are looking for is die + level → 33. So, now we navigate to .subckt 33. In the subckt, you will find a '.func Cgs(V)' statement:

    image.png

    This statement defines the gate-source capacitance across Vgs. To change it to a static capacitance, you can just set the lookup table to a single value:

    image.png

    Now, what this has done is changed Cgs to a single value at 1 nF. So, you can adjust 'ags' like you were before, but it will be adjusting a static capacitance. So, ags = 20 would set the capacitance to 20 nF.

    To measure the capacitance in LTspice, you can use this circuit:

    image.png

    Then implement this equation: 1e3/(2pi1e3*(V(Vgg)/I(V1)))

    image.png

    Note that this circuit measures Ciss(Vgs), which is Cgs + Cgd. To isolate Cgs, you can just set agd = 0 in the Spiceline.

    image.png

    If you look back at our lookup table, we see the entry (-5, 8.83). This means that at Vgs = -5 V, Vgs is 8.83 nF. 5 die in parallel → 44 uF, which matches our plot above.

    Let me know if you have any further questions.

    Thanks,

    Brian

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.