Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

mounting CBB021M12FM3 with PCB

Dalija
Dalija Contributor Level 1
edited January 2025 in Module Products

As the current rating of CBB021M12FM3 is 48amp, while mounting the module with PCB a maximum of 48amp current will flow through the PCB also. So can a PCB handle this much of current? Also what type of pin should be connected in the PCB to takeout the terminals of CBB021M12FM3 to connect with the external circuit?

Comments

This discussion has been closed.