mounting CBB021M12FM3 with PCB

As the current rating of CBB021M12FM3 is 48amp, while mounting the module with PCB a maximum of 48amp current will flow through the PCB also. So can a PCB handle this much of current? Also what type of pin should be connected in the PCB to takeout the terminals of CBB021M12FM3 to connect with the external circuit?
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hi Dalija,
I recommend taking a look at the design files and user guide provided in the CRD25DA12N-FMC reference design, which utilizes the CCB021M12FM3:
There is also an evaluation board for the full-bridge 21 mΩ FM3 that will provide a good example of the recommended PCB layout, copper weight, and layer count:
Best Regards,
Austin C.
0 -
Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
0