Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CRD-22AD12N at lower power & voltage, higher frequency

Nathan
Nathan Contributor Level 1
edited July 2025 in Module Products

I would like to utilize the CRD-22AD12N for rectification and conversion of a variable speed 1kW generator operating between 20Vrms-72Vrms input and 20Hz-200Hz.

Be able to driving the generator (as a motor) at 72Vrms would also be desirable.

Would this module be able to support my requirements?

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • Nathan
    Nathan Contributor Level 1

    I'll also add that the output bus voltage is a parameter we can vary, but ~150V or less would be ideal.

  • Hzz
    Hzz Wolfspeed Employee - Contributor Level 1

    Hello Nathan,

    Sorry, the CRD-22AD12N is not able to support the application as you mentioned, this demo is only able to operate in the specifications that were listed in the User Guide PRD-02282 as below:

    image.png

    Thank you!

This discussion has been closed.