Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

SpeedVal Kit 3phase-board:SCP triggered when switching on upper device

HansJ
HansJ Contributor Level 1

Dear all,

I’m currently using the following products for my research project:


MOD-MB-3P-0900V-40A-N


EVAL-ADUM4146WHB1Z


MOD-PWR-MM-C3M0032120K


I didn’t use the control card — instead, I generate the PWM signals externally.

In my setup, I only need to produce a single voltage pulse. However, I’ve observed something strange:

—When I use the upper device evaluation configuration and switch on the upper device, the gate driver’s red LED turns on, indicating an SCP (short-circuit protection) event.

—When I use the lower device evaluation configuration and switch on the lower device, no SCP error occurs.

I would like to understand why SCP is triggered only when switching the upper device. Could this be related to the measurement configuration, gate driver reference, or bootstrap/isolated supply setup?

Any suggestions or explanations would be greatly appreciated. Thank you very much!

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • Julius_R
    Julius_R Wolfspeed Employee - Contributor Level 3

    Greetings HansJ:

    Do you have the desat/SCP cables connected? If they are not connected, and you don't have the SCP disable jumpers on the 4146 board, that could be the problem. I put an image up showing the SCP cables installed. The gate driver shown is not the 4146 but you would make the connections on the 4146 in a similar fashion. I also attached an image of the 4146 with the SCP disable pin headers circled. Placing a jumper here will disable the SCP feature and you would not need to connect the desat/SCP cable.

    Julius R

    image.png

    image.png
Sign In or Register to comment.