Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CRD25DA12N-FMC: Lowest allowed DC-link voltage

mtrdrv25
mtrdrv25 Contributor Level 1
edited February 20 in General

Hi,

I just bought a CRD25DA12N-FMC and would like to exercise with lowest possible DC-link voltage to start with. Can you please let me know the lowest possible DC-link voltage I can use for my initial evaluation?

Thanks!

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • ChrisN
    ChrisN Wolfspeed Admin - Contributor Level 5

    Hello mtrdrv25,

    There is no strict minimum voltage for the system to start switching. Internally, we have used the unit in demonstrations with a bus voltage of only 50 V. However, this system is designed to be operated at 800 V, so we recommend operating it at elevated voltage when looking at the performance of the inverter and SiC modules.

    Thanks,

    Chris N.

  • mtrdrv25
    mtrdrv25 Contributor Level 1

    Hi Chris,

    Thanks for the explanation. Just wanted to know what voltage I can use for initial testing before operating the inverter at 800V eventually.

This discussion has been closed.