Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

CRD25DA12N-FMC-AFE Firmware and GUI

Options
Stephen
Stephen Contributor Level 2
edited April 28 in Module Products

Hello

Regarding the CRD25DA12N-FMC reference design, I have added CRD25DA12N-FMC-AFE-BOOST and CRD25DA12N-FMC-AFE-EMI, and I intend to use it as a 25kW rectifier with the TMDSCNCD280039C control card. At this point, what modifications do I need to make to the firmware and GUI you provided? If modifications are required, could you provide a detailed explanation on how to proceed? I have little experience in this area and would greatly appreciate your guidance!

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5
    Options

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • ChrisN
    ChrisN Wolfspeed Admin - Contributor Level 4
    Options

    Hello Stephen,

    We provide the firmware for the CRD25DA12N-FMC inverter with a direct link on the website landing page. The Active Front End (AFE) hardware is shown as a demonstration for how the inverter can be easily modified to support other applications. As you already indicated, all the hardware design files for both these design are already available for download on the website landing pages for the designs (CRD25DA12N-FMC-AFE).

    For proper use, the AFE requires locking onto the 480V grid frequency. Unlike the inverter, the AFE must be operated closed loop which requires ABC/DQ0 transformations. This all needs to be performed in the Control Law Accelerator (CLA) of the controller in order to ensure enough compute resources. All our testing has been performed in very controlled environments, with isolation from the grid. We unfortunately do not plan to provide or support the firmware for this design at this time.

    Thanks,

    Chris N.

  • Stephen
    Stephen Contributor Level 2
    Options

    Okay, I understand. Thank you all.

  • ChrisN
    ChrisN Wolfspeed Admin - Contributor Level 4
    Options

    Hello Stephen,

    I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

    Thanks,

    Chris N.

This discussion has been closed.