Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Change Vth of SiC Bare die model in the negavtive Voltage range

kurt_gn
kurt_gn Contributor Level 1

Hello,

my device of interest is the CPM2-1200-0080B.lib. I want to shift the Threshold Voltage of this device by implementing a parameter "Vth_shift"

in the current modified .lib looks like this:

image.png

this .lib works until the shift is negative and the new threshold would be in the negative voltage range. Are there any ideas how ich can shift the ID-VG curve in the negative direction, so that the new Vth < 0 up to -5V for example?

Tagged:

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • Mhusain
    Mhusain Wolfspeed Employee - Contributor Level 3

    Hello,

    The CPM2-1200-0080B die is an N-channel enhancement-mode MOSFET, and the model is built around the assumption that the device threshold voltage is positive. Because of that, introducing a sufficiently large negative Vth_shift such that the resulting threshold becomes negative will likely push the model outside its valid operating range and can break the underlying equations and parameterization.

    In other words, the model is intended to represent a device that is normally off at VGS = 0V, so a negative threshold voltage is not physically consistent with the modeled device. If the threshold is forced below 0 V, the model behavior is no longer representative of the actual device and unexpected simulation results should be expected.

    Therefore, a negative threshold voltage is generally not supported for this model.

    Regards

Sign In or Register to comment.