Double-Pulse Test Waveform Differences: SiC Module vs. Discrete MOSFET
Hi,
I am running a double-pulse test (DPT) using the DPT_Test_Stand_HB example from All SPICE Models\Modules\LTspice\Example Circuits\HalfBridge
I am comparing two cases: one using a SiC power module and another using a discrete SiC MOSFET.
When I zoom in on the switching transient, I can see some differences in the current and voltage waveforms. In the attached figure:
- Left: Shunt current, voltage across the lower switch, and gate signal for the SiC power module.
- Right: The same signals for the discrete SiC MOSFET.
In the literature and examples, the voltage and gate waveforms generally look more similar to the ones shown on the left. However, in the discrete MOSFET case (right), I observe a spike in the gate signal together with a dip in the switch voltage.
Could someone please clarify what is causing this behavior in the discrete SiC MOSFET case? In particular:
- What causes the spike in the gate signal?
- Why does the switch voltage show a corresponding voltage dip?
- Is this behavior expected for a discrete SiC MOSFET, or is there an issue with my model or test setup?
For each case, I have adjusted the load inductance L and the gate resistors Rgon and Rgoff accordingly.
Any explanation of the differences would be much appreciated.
Thank you!
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Dear Wolfspeed Team,
Just following up on this question in case it was missed. It has been a couple of weeks, so I wanted to bring it back to the top.
I would really appreciate any guidance and clarification.
Kind regards
0 -
@Forum_Moderator , any update?
0 -
Hi im_zg,
I checked the models and have built a new model for the device, I believe it was due to the curve fitting parameters that models the channel current. I have also attached the results of the DPT test with the new model.Let us know if you need anything else from us.
Regards
0 -
Hello im_zg,
I will be closing this post for now. Please feel free to create a new post if you have any other questions.
Thank you,
Chad F.
0