Request: LTspice-Compatible SPICE Model for C2M1000170D SiC MOSFET
Hello everyone,
I am currently working on a power electronics design that requires the C2M1000170D SiC MOSFET from Wolfspeed. However, I was unable to find an LTspice-compatible SPICE model for this part on the official Wolfspeed website.
This model is critical for my circuit simulation work in LTspice, so I would greatly appreciate it if anyone in the community could share a valid SPICE model file for the C3M0015065K, or point me to a reliable source where I can obtain it.
Additionally, I would like to inquire whether your company has a 3300V 20A silicon carbide MOSFET product (C2M1000330). I have found a product from another company that has the same name and data parameters as your C2M1000170D product. Therefore, I would like to seek assistance from your company to see if you have a similar 3300V silicon carbide device. If so, could you provide me with your data sheet and LTspice model? I would be very grateful
Thank you very much for your help!
Best regards,
Comments
-
Thank you for your post, it has been approved and we will respond as soon as possible.
0 -
Hello,
Thank you for your interest in Wolfspeed devices.
The LTspice-compatible SPICE models are available in the .zip package below, which includes models for our supported SiC MOSFET portfolio:
You can also get them here "https://assets.wolfspeed.com/uploads/2023/09/Wolfspeed_SPICE_Models.zip"
Regarding the 3.3 kV device, Wolfspeed does not currently offer a 3300 V discrete SiC MOSFET equivalent to the C2M1000330. However, we do offer a 3300 V SiC MOSFET bare die, CPM3-3300-R050A, which has a current rating of 52 A. You can find more information here:
https://www.wolfspeed.com/products/power/sic-bare-die-mosfets/?blockingVoltage=3300%20V
We hope this helps. Please let us know if you have any additional questions.
Regards
0 -
Hello,
I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.
Thanks
0