Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

Rated Temperature of Gate Drive Board

jwei_wolfspeed
jwei_wolfspeed Contributor Level 1
edited April 2023 in Module Products

For the gate drive board CGD1700HB3p-HM3, it has max 85C operating ambient temperature. what is the limit factor for it? Can it be modified to operated at max 105C operating ambient temperature? Thank for help

Tagged:

Comments

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hello, thank you for your message. A member of our technical team is looking into your questions and we will respond shortly. 

  • PaulKanatzar
    PaulKanatzar Wolfspeed Employee - Contributor Level 2

    Hello,


    The MGJ3T12150505MC-R7 power supply is the first limit to 85 °C, at full load it rises 18 °C above ambient leading to a max operating temp of 103 °C two degrees below its rating.


    Forced cooling of the gate driver may help with the ambient temperature limitation. At this time we do not have plans to increase the temperature rating of this particular design.


    Thanks,

    Paul Kanatzar

  • jwei_wolfspeed
    jwei_wolfspeed Contributor Level 1

    Hi Paul,


    Thank for your reply. Can we replace MGJ3T12150505MC-R7 power supply with higher temperature power supply by ourselves? Would it be allowed for us to modify your CGD1700HB3P-HM3 ALL Design Files and make new gate drive board to meet our requirements?


    Thanks,

    Jim Wei

  • PaulKanatzar
    PaulKanatzar Wolfspeed Employee - Contributor Level 2

    Jim,

    You can absolutely modify the design files to meet your needs! That's actually one of our primary goals in providing designs publicly. Feel free to check out our other 1.7 kV reference designs as well for ideas and parts that may suit your needs (CGD1700HB2M-UNA, CGD1700HB2P-BM3_Data_Sheet.pdf" rel="nofollow noopener ugc">CGD1700HB2P-BM3, and CGD1700HB2P-XM3_Data_Sheet.pdf" rel="nofollow noopener ugc">CGD1700HB2P-XM3).

    -Paul

  • TBhatia
    TBhatia Wolfspeed Admin - Contributor Level 5

    Hi, I hope that this answered your question. I will close this discussion for now but if you have a follow up question, please "Start a New Discussion" and we would be glad to support you further.

This discussion has been closed.