Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

LTspice model question: parasitic parameters associated with discrete packages

Hiroshi
Hiroshi Wolfspeed Employee - Contributor Level 2
edited April 2023 in Discrete Products

Hi Wolfspeed experts,


According to the document, LTspice model has a parasitic component associated with the package (gate, source, drain and kelvin). When I check the parameters described in the library file (C3M0016120K.lib for this case), I found:

Ls1 and R_Ls1 : inductance & resistance of source pin & wires

Ls2 and R_Ls2 : inductance & resistance of kelvin pin & wire

Lg and R_Lg : inductance & resistance of gate pin & wire

Ld and R_Ld : inductance & resistance of drain pin & wires


Here's the question, what parameters Rv and Lv and R_gg refer to?


Thank you for your support.

Best Regards,

Hiroshi

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • ZMiller
    ZMiller Wolfspeed Employee - Contributor Level 3

    Hi,

    Lv is the inductance that is common to both the gate loop and power loop in the device. Rv and R_gg are both "convergence aides" that do not reflect device performance but are added to help the solver in LTSpice converge when running a simulation. I hope this helps!

    Thanks,

    Zack

  • Hiroshi
    Hiroshi Wolfspeed Employee - Contributor Level 2

    Hi Zack,

    I get it now. Thank you for the answer!

This discussion has been closed.