Wolfspeed Power Applications Forum

Wolfspeed Technical Community:

PLECS XML file for CAB5R0A23GM4T

Prathik
Prathik Contributor Level 2
edited July 2025 in Module Products

Hello,

Could you share the updated XML file for the CAB5R0A23GM4T power module, the one similar to the XML for the CAB6R0A23GM4T (attached below) which you are developing internally? I am trying to decide which power module to select between the two for my project, and the updated XML file will help me with this.

Regards,

Prathik

Comments

  • Forum_Moderator
    Forum_Moderator Wolfspeed Employee - Contributor Level 5

    Thank you for your post, it has been approved and we will respond as soon as possible.

  • BlakeNelson
    BlakeNelson Wolfspeed Employee - Contributor Level 3

    Hi Prathik,

    I've attached the integrated models for all three 2300V Wolfpacks. Let me know if you need anything else!

    Thanks,
    Blake

  • Prathik
    Prathik Contributor Level 2

    Thank you very much, Blake!

  • Prathik
    Prathik Contributor Level 2

    Hello Blake,

    I have a question about the XML file. I noticed that the diode reverse recovery losses are not modelled (both in the XML which you shared in this thread and in the XML that are already available in the WS website). This is not specific to the CAB5R0 part and I've noticed that in a lot of WS XMLs, the Err information of the diode is blank. Is there any specific reason for this?

    image.png

    The Err information is available in the datasheet. Although it is smaller than Eon and Eoff when Ids>150A, it is definitely significant for lower values of Ids.

    image.png

    Please let me know what you think about this.

  • BlakeNelson
    BlakeNelson Wolfspeed Employee - Contributor Level 3

    Hi Prathik,

    I do have some experimental models with the Err losses included for the 2300V wolfpacks. The Err loss table is a recent development and we are working on validation, any feedback you have would be appreciated! (Sorry to make you a beta tester)

    My hope is that we can release our new models with all the recent improvements to our website this year (though many older parts are missing the full dataset required to add all the model features included in these ones). Until then, feel free to reach out on the forum and I can provide whatever model is latest for a specific part.

    Thanks,
    Blake

  • Prathik
    Prathik Contributor Level 2

    This helps. Thank you, Blake!

This discussion has been closed.